alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Ensuring Hydrogen Purity for Fuel Cells

Sampling at the nozzle is critical to ensuring hydrogen purity for PEM fuel cells

Why Sampling at the Nozzle Matters for Reliable, Standards-Compliant Hydrogen Systems

As the global energy landscape shifts toward cleaner and more sustainable solutions, hydrogen has become a pivotal fuel for decarbonizing transportation, industry, and power generation.

Among its most promising applications is the use of hydrogen in proton exchange membrane (PEM) fuel cells, which offer high efficiency and zero emissions for vehicles and stationary systems. However, the performance, safety, and longevity of fuel cells are critically dependent on the purity of hydrogen supplied—a requirement that is far more stringent than other industrial uses. Even trace levels of contaminants can cause irreversible damage, reduced operational efficiency, and compromised system reliability.

Sauhaib Filali, Application Engineer at Swagelok Munich
Sauhaib Filali, Application Engineer at Swagelok Munich

Ensuring hydrogen purity is not simply a matter of laboratory analysis; it demands a comprehensive approach that spans the entire value chain—from production and storage to transfer and dispensing. At each stage, hydrogen is vulnerable to degradation and contamination, making robust sampling and verification procedures essential.

In response to this environment, Sauhaib Filali, an application engineer at Swagelok Munich, who specializes in the clean energy market, authored this white paper as a technical guide for engineers, operators, and stakeholders involved in hydrogen infrastructure and fuel cell deployment. It explores the principles and engineering challenges of hydrogen sampling, reviews the relevant standards, and presents practical system architectures that support accurate and compliant fuel quality verification.

Read the Whitepaper

In this question-and-answer session, Sauhaib takes the time to explain the market, the reasons behind this white paper, and how it can help customers.

Q: Tell us about yourself and how you came to work in this industry.

A: I completed my first bachelor’s degree in mechanical engineering from Hassan II University of Casablanca (Morocco) in a French-language engineering program. But I was motivated to deepen my technical expertise and build an international engineering career, so I moved to Germany and earned a second bachelor’s degree in mechanical engineering from the University of Applied Sciences Berlin, where the curriculum is taught in German.

In my current role at Swagelok Munich, which I started in 2022, I support the design, documentation, and implementation of hydrogen fluid systems across the entire clean-energy value chain, including hydrogen production, distribution, storage, sampling, and on-vehicle applications. My work spans process engineering, P&ID development, component specification, developing 3D system models and assembly drawings, and onsite technical support for customers.

Additionally, I evaluate systems and components for compliance with international hydrogen regulations to ensure safe, standards-aligned system designs. And I regularly speak at industry events such as Hannover Messe and TankTech on hydrogen system design best practices, hydrogen fuel quality, sampling and safety standards.

Q: How do you see the hydrogen market, both now and in the future?

A: In my role as an application engineer, I’ve witnessed the global hydrogen market evolve rapidly. It has moved from bold political ambitions and early-stage experimentation to a more structured, standards-driven deployment phase. Electrolyzer capacity has grown significantly, and fuel-cell mobility is starting to gain traction across Asia and Europe.

Europe’s approach has especially impressed me, as it includes binding infrastructure targets. For example, the European Union’s Alternative Fuel Infrastructure Regulation (AFIR) regulation requires hydrogen refueling stations to be available every 200 kilometers along core transport routes by 2030.

That said, the market still faces real challenges. One of the biggest is the gap between deployment and reliability. Too many systems are being built without consistent attention to fuel quality or long-term durability. Hydrogen fuel cells are highly sensitive to trace-level contamination, and quality assurance was, until recently, often overlooked.

Now, I’m encouraged to see the industry addressing this. New standards like ISO 19880-9 are finally providing clear guidance for hydrogen sampling at the dispenser, helping ensure that what reaches the vehicle meets critical purity specifications. I’m optimistic that this shift will carry the hydrogen economy toward scalable, long-term success.

Q: What did you see in the industry that made you author this white paper?

A: I see a critical gap in how the industry understands hydrogen fuel quality requirements for PEM fuel cell stacks and the role of sampling in protecting them. Hydrogen fuel must be at least 99.97% pure, with only trace contaminants allowed. But many customers were unsure how to achieve that level of purity at the point of dispensing. Many were/are relying on the supplier’s certificate of analysis, without realizing that hydrogen quality can degrade during compression, storage, and dispensing.

Sampling is an essential engineering approach to verify that the hydrogen still meets the required specifications at the point of use. However, sampling is a complex process, and if it’s not done properly, it can lead to inaccurate results, non-compliance, or long-term damage to the system.

Q: What are some of the most important hydrogen standards customers need to be aware of?

A: There are several hydrogen standards I think every customer working with fuel cell systems should know to ensure hydrogen quality for a safe and reliable operation. I will explain it in terms of three key levels that need to work together: what needs to be measured, how the sample is taken, and how it’s analyzed.

At the first level, ISO 14687 (and in some regions SAE J2719) defines the hydrogen fuel quality requirements, including the maximum allowable limits for critical impurities. Then at the second level, we have standards like ISO 19880-9 and ASTM D7606-17, which cover how to take a proper hydrogen sample at the dispenser, including everything from purging and grounding to material compatibility. The third level is about analysis: ISO 21087 outlines which analytical methods to use in the lab and how to keep the sample stable during transport.

The key point is that these three levels must match. A system might be technically well-built, but without sampling that aligns with the right standards, the purity result won’t be trustworthy.

Q: What is the single-biggest engineering challenge when it comes to hydrogen sampling?

A: In my experience, it’s maintaining sample integrity. That means ensuring the sample truly represents the actual hydrogen composition from extraction to analysis. It sounds straightforward, but even tiny leaks, a bit of residual gas trapped in a dead leg, or incomplete purging can introduce contaminants or dilute the impurities we’re trying to measure. As a result, the sample no longer reflects what’s really in the hydrogen stream.

Overcoming this requires designing the sampling system properly, starting with compatible materials, eliminating dead volume, and ensuring thorough purging. Only then can we be confident that the hydrogen reaching the analyzer is as pure and unchanged as it was at the source.

The system is only as clean as its sampling process. Even high-purity hydrogen can be compromised by a poorly designed or executed sampling method, allowing contamination or an unrepresentative sample to invalidate your results.

That’s why we must design the sampling system with the same care and adherence to international standards as the rest of the hydrogen fuel system. In practice, sampling isn’t just an analysis approach; it’s a critical system-level decision that directly impacts fuel cell performance and safety.

Q: If a customer remembers only one thing from this white paper, what do you want it to be?

A: If you only take one thing from this white paper, I hope it’s that fuel quality at the nozzle is what truly matters. Even if hydrogen leaves the production plant pure enough, it can pick up contaminants during the hydrogen chain value. That’s why we have to test it right at the nozzle to ensure the fuel cell gets exactly what it needs.


“Hydrogen sampling isn’t just a secondary consideration—it plays a vital role in safeguarding the fuel cell.”
- Sauhaib Filali, Swagelok Munich

hydrogen icon 
 

Read Sauhaib’s white paper “Ensuring Hydrogen Purity for Fuel Cell Applications.” If you have questions about hydrogen sampling, contact your local authorized Swagelok sales and service center for assistance.

Contact a Local Specialist