alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Make FEED Decisions That Carry Forward

Align scope, specifications, and material choices early to reduce downstream risk and improve execution outcomes.

Connect with your local team

 Back to Global Construction


Front End Engineering Design (FEED) Support for Capital Projects


The Front-End Engineering Design (FEED) stage is where early intent becomes defined scope. Requirements are clarified, assumptions solidify, and decisions made here begin to shape cost, schedule, and execution.

Swagelok supports you during FEED by bringing fluid system expertise into this decision‑making phase. Because we stay involved beyond FEED and into detailed design, construction, and commissioning, we help ensure choices made now can be carried forward smoothly as the project progresses.

Contact a Specialist

  line

Why the FEED Stage Is Critical to Capital Project Success

Decisions made during the FEED stage strongly impact capital project outcomes Decisions made during the FEED stage have a disproportionate impact on overall project outcomes. Early choices around scope definition, specifications, and material selection directly influence cost certainty, schedule confidence, and how smoothly a project transitions into execution.

Swagelok supports you during this phase by bringing fluid system expertise into early decision-making—helping ensure that what is defined during FEED is practical, aligned, and ready to carry forward. By providing insight into material selection, availability, and system design considerations, we help reduce uncertainty while changes are still manageable.

When FEED inputs are well defined and supported, teams can move forward with clearer procurement strategies, stronger alignment across stakeholders, and fewer surprises during detailed design and construction. Conversely, when FEED is rushed or incomplete, gaps often surface later—when changes are more complex, costly, and disruptive.

By engaging early and remaining involved beyond FEED, Swagelok helps you create a more stable foundation for execution—supporting continuity from initial design through construction and commissioning.

How Swagelok Supports You During the FEED Stage

Learn how Swagelok can support you during the FEED stage of your capital projectDuring FEED, teams are defining scope boundaries, pressure‑testing specifications, and making early decisions that directly affect cost, constructability, and execution risk. Swagelok works alongside owners, EPCs, engineering consultants, and package vendors to help ensure fluid system decisions made during FEED support executable designs, reliable estimates, and a smoother transition into detailed design and procurement—helping you achieve on-time commissioning with the quality your asset requires.

What you can expect when working with Swagelok:Swagelok works alongside owners, EPCs, engineering consultants, and package vendors during FEED

  • Early visibility into lead times and availability. We help identify long-lead components and plan around procurement constraints.
  • Support for quantity validation and top-off strategies. We help align estimates with realistic installation and commissioning needs.
  • Early FEED-stage insight. We help you identify fluid-system-related considerations while adjustments are still manageable.
  • Support for clear scope definition. Our involvement helps clarify fluid system boundaries so FEED outputs are usable for EPC bidding and execution.
  • Alignment across stakeholders. We support coordination between owner standards, EPC requirements, engineering consultants, and package vendors.
  • Lifecycle‑aware decision support. We help you consider constructability, availability, and long‑term operability—not just initial design intent.
  • Global consistency with local engagement. Support is delivered through Swagelok’s global network while working directly with local project teams.

Common Mistakes to Avoid During the FEED Phase

Avoid common FEED mistakes in your capital projectEven well-planned projects can experience downstream challenges when early FEED decisions are incomplete or misaligned. Common issues include underdefined scope boundaries that lead to change orders during detailed design or construction, as well as incomplete material and component selections that result in late-stage substitutions or procurement delays.

Limited visibility into lead times early in the process can introduce unnecessary schedule risk, while gaps between FEED deliverables and EPC expectations can affect bid quality and execution readiness. Addressing these areas during FEED helps reduce downstream disruption and supports more predictable project outcomes.

Key Focus Areas During FEED

Focus areas for the front-end engineering design phase of your capital projectScope Definition and FEED Deliverables

FEED deliverables form the foundation for procurement and execution. Swagelok helps you strengthen fluid‑system‑related inputs so they are clear, aligned, and ready to carry forward.

How we support you:

  • Input into fluid system design basis and specifications
  • Review of P&IDs and component selection assumptions
  • Identification of gaps that may affect EPC RFQs or execution readiness

Material Selection and Component Selection Strategy

Material and component decisions made during FEED influence cost, availability, and long‑term performance. Swagelok helps you evaluate options against service conditions and lifecycle considerations before they become fixed in procurement packages.

How we support you:

  • Evaluation of material and component tradeoffs
  • Support for standardization strategies to reduce complexity
  • Early identification of long-lead or higher-risk selections
  • Interpret specifications and compliance requirements

Risk, Change, and Handover Readiness

FEED is the right time to surface and address potential issues while flexibility still exists. Swagelok supports engineering‑led risk and change discussions by bringing fluid‑system‑specific insight into FEED reviews and handover planning.

How we support you:

  • Input into safety‑in‑design and HAZOP discussions
  • Identification of interface and execution considerations tied to fluid systems
  • Support for documentation clarity to enable smoother EPC handover
line

Supporting Execution Beyond FEEDSwagelok provides global support, locally

Swagelok’s involvement doesn’t end when FEED is complete. Because we continue to support projects through detailed design, construction, and commissioning, we help maintain continuity as FEED decisions move into execution—supporting smoother transitions and fewer downstream disruptions.

When scope is being defined and decisions are still flexible, early input has the greatest impact.

Talk with Swagelok about your project