Why You Should Avoid Intermixing and Interchanging Tube Fittings
Selecting the right tube fitting components is critical to maintaining fluid system reliability, safety, and performance. While some manufacturers claim their tube fitting components are interchangeable with other brands, mixing or swapping fitting components from different manufacturers can introduce significant risks that may not be immediately apparent.
In this video, you'll learn the difference between intermixing and interchanging tube fittings and why these practices can lead to unpredictable performance, increased maintenance costs, leaks, and potential safety hazards. Because tube fitting manufacturers use their own proprietary designs and specifications, components from different brands are not necessarily engineered to work together. As a result, combining fitting bodies, nuts, or ferrules from multiple manufacturers can create an assembly with unknown performance characteristics.
You'll also discover why many fluid system professionals recommend sourcing tube fittings from a single manufacturer to help ensure consistent performance, maintain warranty coverage, and reduce the risk of leaks, environmental releases, and unplanned downtime. Understanding the risks associated with intermixing and interchanging fittings can help you make informed decisions that support long-term system integrity, operational efficiency, and workplace safety.
Video Transcript
Critical fluid systems rely on dozens of quality components working harmoniously to keep operations running efficiently. Any performance lapses can result in leaks, potential safety concerns, and system downtime. One way to prevent these issues is to always build your fluid systems with tube fittings from a single manufacturer.
Let's explore why interchanging and intermixing tube fittings from different manufacturers can lead to poor fluid system performance.
Interchange is when a tube fitting from one manufacturer that has been installed on a piece of tubing is disassembled, and the tubing, nut, and ferrules are then reassembled into a tube fitting body from another manufacturer.
Intermix is when tube fitting components, including the nuts, ferrules, and bodies from two or more manufacturers, are mixed together and then assembled to make a completed fitting.
Why can interchange and intermix be problematic? Importantly, there is no industry-wide design standard for tube fittings, unlike NPT, SAE, or cone and thread fittings, which do have recognized design standards that enable intermixing of those fittings. This means that every individual manufacturer follows its own design standards and processes for tube fittings. Therefore, tube fitting components from different manufacturers are not designed to work together, and an intermixed or interchanged fitting is essentially a new, unknown design.
Some manufacturers may claim that their products are interchangeable with other brands, but how can any manufacturer reliably, repeatedly, and uniformly replicate designs of a competitor?
For these reasons, interchanging and intermixing tube fitting components can lead to unpredictable performance, higher long-term costs, unintentional environmental releases causing environmental harm, and potential safety hazards. Intermix and interchange may also void the manufacturer’s warranty, which can lead to even higher costs if or when a problem occurs due to intermix or interchange.
Avoiding intermix and interchange is a best practice promoted by numerous fluid system standards organizations and specifications. Single-sourcing your tube fittings from one reliable supplier is a good way to avoid potential interchange and intermix, even by accident. When only one brand is available, technicians can't mistakenly combine components from two different manufacturers.
For more information about tube fitting installation, visit swagelok.com or contact your local authorized Swagelok Sales and Service Center.