MPC Configurator
Swagelok Modular Platform Components (MPC) Configurator
The MPC Configurator is an interactive tool to build and assemble ANSI/ISA 76.00.02-compliant miniature modular designs prior to the purchase process.
To download and install the Swagelok MPC Configurator:
- 
    Please select the version of the MPC Configurator that you would like to download:
    
- 32-bit version: Swagelok MPC Configurator 2.4 — 32-bit
 - 64-bit version: Swagelok MPC Configurator 2.5 — 64-bit
 
- The program file is 99 MB
 - The configurator is in English
 - The program is a self-extracting zip file
 
 - Double-click the MPC Configurator Installation file. The install process will begin.
 - At the MPC Welcome screen, select "Next."
 - At the License Agreement screen, you will need to Agree to the license agreement and select “Next” to continue.
 - The installation process will put the MPC configurator files in a folder called "C:\Program Files\Swagelok\MPC Configurator 2.4". If you want to use the default folder, then click the “Next” button. If you want to put the files in a different folder, click "Browse" button and select another folder. When finished, click the “Next” button to proceed.
 - Click “Next” to start the install.
 - The files are copied and registered on your computer. The next screen indicates Swagelok MPC setup was completed successfully. Select “Close” to complete the process.
 
| System Requirements: | 
| The configurator is in English only at this time. | 
| The zip file is 97 MB. | 
| 150 MB hard disk space needed. | 
| Microsoft Windows XP, Microsoft Windows Vista (any version), or Microsoft Windows 7 (any version) | 
| .NET 3.5.1 Framework | 
| CAD Output Requirements: For AutoCAD Output: AutoCAD 2010 (Lite version will NOT work) For SolidWorks output: SolidWorks 2007, 2008, 2009, 2010, 2011, or 2012  | 
        
Frequently Asked Questions (FAQs) about the Swagelok MPC Configurator
Below is a list of frequently asked questions regarding the locally installed Swagelok MPC Configurator application. This FAQ covers the system requirements and technical issues for the configurator. Any questions on general use of the software are covered in the help file included with the software.
Question: What is the Swagelok MPC Configurator?
Answer: The Swagelok MPC Configurator is a software application with an easy-to-use interface for designing sampling systems in the modular format. The output is a complete bill of materials and an assembly schematic that details the exact placement of each individual component in the system construction. In addition, the configurator can provide basic engineering calculation functions along with AutoCAD & SolidWorks outputs.
Question: What are the base software requirements for the Swagelok MPC Configurator?
Answer: To use the basic configurator functions, excluding CAD outputs, the software requirements are:
- Microsoft Windows XP (any version), Microsoft Windows Vista (any version), or Microsoft Windows 7 (any version)
 - Microsoft .NET 4.0 Framework
 
Question: What are the software requirements for the CAD outputs of the Swagelok MPC Configurator?
Answer: In addition to the base software requirements, CAD outputs from the MPC Configurator require:
- For AutoCAD output: AutoCAD 2010 (Lite version will NOT work)
 - For SolidWorks output: SolidWorks 2007, 2008, 2009, 2010, 2011, or 2012
 
Question: What are the hardware requirements for the Swagelok MPC Configurator?
Answer: There are no specific hardware requirements for the MPC Configurator.
Question: What user account permissions are needed to install the MPC Configurator?
Answer: The MPC Configurator must be installed with an account with Administrator privileges.
Question: What user account permissions are needed to run the MPC Configurator?
Answer: The MPC Configurator can be run by a user with a limited account.
Question: I am having an issue installing a newer version of the MPC Configurator or completing an update of the Configurator from swagelok.com.
Answer: Completely remove the old version of the MPC Configurator from your system, and then complete a new installation using the latest version of the MPC Configurator (available on swagelok.com).
Question: Where can support for the MPC Configurator be obtained?
Answer: Support for the MPC Configurator is available through your local authorized Swagelok sales and service center.