alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Understanding How Regulators Function


Pressure regulators play a vital role in maintaining stable, controlled pressure throughout fluid systems. By balancing internal forces, regulators help ensure that gases and fluids are delivered at the desired pressure, helping protect equipment, support process consistency, and promote safe operation. In this video, you'll learn the basic principles behind regulator operation, including the functions of the sensing, loading, and control elements and how they work together to achieve pressure control. Understanding how regulators function can help improve system performance and reduce the risk of downtime or product quality issues. Read more about How to Choose a Regulator. 

Find a local expert

Video Transcript


The basic function of a regulator is to control pressure reliably and consistently. You take the upstream pressure and regulate it down to a downstream pressure, which then provides the system with a consistent flow for it to operate. A pressure regulator is used in many different systems to control either downstream or upstream pressure as other things within the system change—whether that's flow demand, temperature, or usage of different components elsewhere in the system. The regulator works to maintain those pressures as all of that changes.

Pressure regulators are built with many different components, but there are three groups that drive regulator performance. The first is the control element: the poppet and the seat that control how much pressure drop happens between the high- and low-pressure sides.

The second is the loading element—most often a spring, though sometimes a pressurized dome of gas. This is the part the user interacts with. As we turn the handle one way or another, we compress the spring or allow it to relax, changing the forces inside the pressure regulator.

The third is the sensing element. This is usually a diaphragm or a piston. It senses what is happening downstream—how much pressure there is—and allows the poppet to know what position it needs to be in to optimize performance.

The key function of a regulator is to control pressure, and that is done by a balance of forces within the regulator. We apply a load—either from a spring or from a diaphragm and a dome with pressure inside it—which gives us downward force.

The pressure coming into the regulator goes past a small poppet that is in contact with, or nearly in contact with, the seat. There is a very fine gap. That fine gap causes the pressure above the poppet to be reduced from the pressure below. The pressure above the poppet acts on a sensing chamber. A sensing element—a diaphragm or piston—is pushed upward, balancing the force from the spring pushing downward. When those forces reach a balance point, the regulator reaches a state of equilibrium and operates at its set pressure.

Regulator performance is critical because it directly influences the customer’s process. Equipment or analytical systems depend on where the regulator is installed. The customer needs the regulator to maintain outlet pressure as close as possible to the required specification.

If the regulator does not function properly, it could damage equipment upstream or downstream. When a regulator isn’t operating optimally, it affects the customer’s end process—production, product quality, purge times, or even component failure due to inconsistent pressures.

Customers may experience downtime if the regulator does not perform as expected. The regulator is often a key element within the customer’s system, and it must function properly to ensure the entire system operates as it should.